Technical FAQs

Ask a Question

What are the no. of electrical operating cycles of Acti9 DPNa circuit breaker.

The no. of electrical operating cycles of Acti9 DPNa circuit breaker are given below:

Electrical Endurance
-> Less than equal to 20 A -  20,000 cycles
-> greater than equal to 25 A - 10,000 cycles
Was this helpful?
What can we do to improve the information ?