Technical FAQs

Ask a Question

What is the operating and storage temperature of Acti9 DPNa circuit breaker.

The operating and storage temperature of Acti9 DPNa circuit breaker is given below:

-> Operating temperature -35°C to +70°C
-> Storage temperature -40°C to +85°C
Was this helpful?
What can we do to improve the information ?