Technical FAQs

Ask a Question

Is plug in base of NS and NSX are compatible and is it possible to install NSX + Vigi device on NS plug in base.

Concerning the basic frame configuration of the plug-in base and the MCCBs,  NS and NSX are fully compatible. NSX  + Vigi device can be installed on a NS plug in base or vice-versa.
But they are not compatible regarding the auxiliaries wiring.  The position of the auxiliaries signals are not the same on NS and NSX.
Was this helpful?
What can we do to improve the information ?