Technical FAQs

Ask a Question

What is the function of iRLI changeover relay.

This relay helps in relaying of ON or OFF information to the auxiliary circuits and actuation of low-power loads.
The iRLI relay contains 1 changeover contact (O-C) and 1 normally open contact (N/O).
Was this helpful?
What can we do to improve the information ?