Technical FAQs

Ask a Question

What is the operating control voltage range for PM5500 series meter.

The operating control voltage range for PM5500 series meter is "100-480 V AC ±10% CAT III 600V class per IEC 61010".
Was this helpful?
What can we do to improve the information ?