Technical FAQs

Ask a Question

What is the maximum Load voltage/current of Digital Output for PM5500 series meter.

The maximum Load voltage of Digital Output for PM5500 series meter is 30 V AC / 60 V DC and current is 125mA.
Was this helpful?
What can we do to improve the information ?