Technical FAQs

Ask a Question

What is the voltage rating (Ue) and control voltage (Uc) of changeover relay iRLI.

The voltage rating (Ue) and control voltage (Uc) of changeover relay iRLI is given below

Ue -> iRLI is available in different voltage ratings of 230…240VAC , 48VAC , 24VAC & 12VAC.
Uc -> 230VAC
Was this helpful?
What can we do to improve the information ?