Technical FAQs

Ask a Question

What is the Input burden of Status input for PM5300 meter.

The Input burden of Status input for PM5300 meter is 2mA @24V DC.
Was this helpful?
What can we do to improve the information ?