Technical FAQs

Ask a Question

What is the Input burden of Status input for PM5500 meter.

The Input burden of Status input for PM5500 meter is 2 mA@24V AC/DC.
Was this helpful?
What can we do to improve the information ?