Technical FAQs

Ask a Question

If Masterpact draw-out breaker is connected directly to Modbus network (without I/O module, IFM or IFE), what are the disadvantanges of this setup.

If CCM or IO Module is not used, So when breaker is withdrawn, it disappears from the Modbus line and the supervisory system will report a time out alarm.
Was this helpful?
What can we do to improve the information ?