Technical FAQs

Ask a Question

Is the tripping curve for EZC DC and AC application the same.

Tripping Curve of both breakers is same. For Example, EZC100F breaker can be used for 550V AC and 250V DC. So tripping curve will be same for DC and AC Application.
Was this helpful?
What can we do to improve the information ?