Technical FAQs

Ask a Question

What is the degree of protection (IP) of iRLI changeover relay.

The degree of protection (IP) of iRLI changeover relay (device only) is IP20.
Was this helpful?
What can we do to improve the information ?