Technical FAQs

Ask a Question

What is the function Extra low voltage (ELV) iRTBT interface relay.

The iRTBT relay actuates LV circuits based on an extra low voltage order. ELV orders can be issued by a programmable logic controller (24 V DC static outputs), a central fire detection unit, a regulation system, etc.
Was this helpful?
What can we do to improve the information ?