Technical FAQs

Ask a Question

What is the input control voltage (Uc) of extra low voltage iRTBT interface relay.

The input control voltage (Uc) of extra low voltage iRTBT interface relay is 

-> 12...24 VAC, -15 to +10 %
-> 12...24 VDC, ±20 %
Was this helpful?
What can we do to improve the information ?