Technical FAQs

Ask a Question

What is the degree of protection of extra low voltage iRTBT interface relay.

The degree of protection of extra low voltage iRTBT interface relay is IP20 (device only).
Was this helpful?
What can we do to improve the information ?