Technical FAQs

Ask a Question

What is the IEC standards to which of Acti9 extra low voltage interface iRTBT relay conforms to.

The Acti9 extra low voltage interface iRTBT relay conforms to IEC 255 100 and IEC 529 standards.
Was this helpful?
What can we do to improve the information ?