Technical FAQs

Ask a Question

What is the maximum value of resistance and capacitance which can be displayed on XM300.

The maximum value of resistance is 999Kohm and for capacitance is 999microF.
Was this helpful?
What can we do to improve the information ?