Technical FAQs

Ask a Question

There is no display observed in ATS22 Soft Starter when Power up the ATS22 Soft starter, what will be the probable reason.

The most probable reason could be too high input voltage on CL1-CL2.
Was this helpful?
What can we do to improve the information ?