Technical FAQs

Ask a Question

What is the part number of contactor which is used in LFM part number VW3A7261 of AFE.


The AFE (Active Front End) consists of a set of three modules installed upstream of the drive between the line supply and the motor.
It is made up of the following elements:
(1) A line filter module (LFM) 
(2) A line filter choke (LFC) 
(3) An active infeed converter (AIC) 

Regarding LFM part number VW3A7261, there are two contactors (K1 & K2) inside the VW3A7261. 

Contactor Components “K1” 
Contactor including 48VDC Coil: LC1F185ED
Auxiliary contact block: LADN22
Terminal Covering: LA9F702

Contactor “K2”: LC1D09BD
Was this helpful?
What can we do to improve the information ?