Technical FAQs

Ask a Question

What is the material of Limit switch head ZCKD08 spring.

The head spring is in stainless steel closed to SUS302 or AISI302.
Was this helpful?
What can we do to improve the information ?