Technical FAQs

Ask a Question

Is it possible to connect single common Line choke for 12 numbers of ATV71 drive.

Line chokes are used to provide improved protection against overvoltages on the line supply and to reduce harmonic distortion of the current produced by the drive.

It is not recommended to connect single common line choke for 12 numbers of ATV71 drive. 
Use separate choke for each drives.
Was this helpful?
What can we do to improve the information ?