Technical FAQs

Ask a Question

Is "Harmony XB5R ZBRN1 (Access Point)” supports Modbus/TCP protocol.

The access point ZBRN1(Wireless access point) has an empty slot for the ZBRCETH communication module to support Modbus/TCP protocol. So, for Modbus/TCP protocol, use ZBRCETH communication module with ZBRN1.
Was this helpful?
What can we do to improve the information ?