Technical FAQs

Ask a Question

What is the Maximum transient current for ATV71 drives.

Maximum transient current for ATV71:
150% of the nominal drive current for 60 second 
165% of the nominal drive current for 2 second 
Was this helpful?
What can we do to improve the information ?