Technical FAQs

Ask a Question

What is the operating control voltage range for PM5300 series meter.

The operating control voltage range for PM5300 series meter is "100 - 277 V AC L-N / 415 V L-L +/-10% CAT III 300V class per IEC 61010".
Was this helpful?
What can we do to improve the information ?