Technical FAQs

Ask a Question

What is the UL acceptability condition for Enerlin'x FDM128.

The Enerlin'x FDM128 display unit is suitable for use in hazardous locations in accordance with Class 1, Division 2
standards. All relevant local, state, and regional codes must be followed.
Was this helpful?
What can we do to improve the information ?