Technical FAQs

Ask a Question

What type of measurement IM400 perform.

Vigilohm IM400 is designed:
a) to monitor the IT power system insulation,
b) to measure:
c) the insulation resistance R (Ω) continuously,
d) C, which is the leakage capacitance of the distribution system to    ground (μF),
e) to calculate the impedance Zc (kΩ) associated with C.
Was this helpful?
What can we do to improve the information ?