Technical FAQs

Ask a Question

What are the frequency setting available in IM400.

This is the rated frequency of the monitored power system.
4 settings are available for the Frequency parameter:
a) DC
b) 50 Hz
c) 60 Hz
d) 400 Hz
Was this helpful?
What can we do to improve the information ?