Technical FAQs

Ask a Question

What is the protection class for varlogic NRC12.

The protection class for varlogic NRC12 is IP41(front panel), IP20(rear part).
Was this helpful?
What can we do to improve the information ?