Technical FAQs

Ask a Question

Is EasyPact SPS EMC ( Electomagnetic compatibility) compliant.

EasyPact SPS devices are protected against:
> Overvoltages caused by devices that generate electromagnetic disturbances
> Overvoltages caused by atmospheric disturbances or by a distribution-system outage (e.g. failure of a lighting system)
> Devices emitting radio waves (radios, walkie-talkies, radar, etc.)
> Electrostatic discharges produced by users

EasyPact SPS devices have successfully passed the electromagnetic-compatibility tests (EMC) defined by the following international standards:
> IEC 60947-2, appendix F
The above tests guarantee that:
> No nuisance tripping occurs
> Tripping times are respected
Was this helpful?
What can we do to improve the information ?