Technical FAQs

Ask a Question

Is Line Load reversibility available in EasyPact SPS circuit breaker.

The Line or Load can be connected to either side of the EasyPact SPS circuit breaker without any reduction in performance.
Was this helpful?
What can we do to improve the information ?