Technical FAQs

Ask a Question

Is EasyPact SPS circuit breaker suitable for isolation.

Yes, the EasyPact SPS circuit breaker suitable for isolation as per IEC 60947-2 standard.
Was this helpful?
What can we do to improve the information ?