Technical FAQs

Ask a Question

What are the Technical specifications of ON/OFF indiaction contacts (OF) of EasyPact SPS circuit breaker.

The Indication contacts indicate the ON or OFF position of the circuit breaker:
>  These OF are rotary type changeover contacts which are directly driven by the mechanism for EasyPact SPS. These contacts trip when the minimum isolation distance between the main circuit-breaker contacts is reached. 




 
Was this helpful?
What can we do to improve the information ?