Technical FAQs

Ask a Question

What are the characteristics of Electric motor MCH of EasyPact SPS circuit breaker.

The electric motor automatically charges and recharges the spring mechanism when the circuit breaker is closed. Instantaneous reclosing of the breaker is thus possible
following opening. The spring-mechanism charging handle is used only as a backup if auxiliary power is absent.
The electric motor MCH is equipped as standard with a limit switch contact CH that signals the “charged” position of the mechanism (springs charged).



 
Was this helpful?
What can we do to improve the information ?