Technical FAQs

Ask a Question

What is the Load burden of Current inputs of ION7650 meter.

The Load burden of Current inputs of ION7650 meter is 0.05 VA per phase (at 5 A standard)and 0.015 VA per phase (at 1 A optional).
Was this helpful?
What can we do to improve the information ?