Technical FAQs

Ask a Question

What are the available communication protocols supported by ION7650.

The ION7650 supports below protocols:
a) Modbus RTU and Modbus Master
b) DNP 3.0
c) GPS
d) EtherGate
e) ModemGate
f) SNMP (this TCP/IP protocol is not set with the Protocol register)
g) IEC 61850 (this TCP/IP protocol is not set with the Protocol register)
h) ION
Was this helpful?
What can we do to improve the information ?