Technical FAQs

Ask a Question

Is it possible to have same device ID of multiple LTMR with same master controller (PLC)

It is not possible to have same device ID for multiple LTMR device with single Master controller (For Ex. PLC).
There will be conflict in exchanging data with the device and more important this configuration is not possible, beacause system will give error.
Multiple devices on single network cannot having same device ID.
Was this helpful?
What can we do to improve the information ?