Technical FAQs

Ask a Question

aM type of Fuse DF2** is fast blow or slow blow type of fuse

aM fuses of DF2** range are slow acting fuses because they allows temporary and harmless inrush currents to pass without opening, but 
is so designed to open on sustained overloads and short circuits.They are generally used in Motor application

 
Was this helpful?
What can we do to improve the information ?