Technical FAQs

Ask a Question

What are different type of connections possible in Com'X 510

There are 3 types of connection possible in com'X 510.
> Modbus over RS485 serial line 
> Modbus TCP/IP over Ethernet 
> Zigbee wireless digital
Was this helpful?
What can we do to improve the information ?