Technical FAQs

Ask a Question

For The Compact NSX DC PV,are the TMD DC trip units adjustable. If TMD DC trip units are adjustable, What are the regulations.

The TMD DC trip units TM DC 80 to TM DC 250 have adjustable threshold from 0,7 to 1 In.These trip units can be used at 1000 Vdc.
Was this helpful?
What can we do to improve the information ?