Technical FAQs

Ask a Question

What is definition of conditional Short Circuit Current.

 Conditional short-circuit current is defined as the value of the current component of a prospective current, which a switch without integral short-circuit protection, but protected by a suitable short circuit protective device (SCPD) in series, can withstand for the operating time of the current under specified test conditions.
Was this helpful?
What can we do to improve the information ?