Technical FAQs

Ask a Question

Is it possible to use NSX 250DC MCCB without trip units as switch disconnector

It is forbidden to use the frame NSX250DC frame without trip unit, even as a switch disconnector use.
NSX100-250NA switch disconnector are self-protected by their high-set magnetic release. 
Was this helpful?
What can we do to improve the information ?