Technical FAQs

Ask a Question

What is the property for 3 leads (wires) used in ref.47849.

Property of 3 leads used in ref 47849 is 
1. Type of wire - Tinned Copper 
2. Size of Wire - 22 AWG 
3. Construction (No. X Ø mm) - 7 X 0.254. 
4. Nominal Voltage - 600 V 
5. Current - 8.51 A 
Was this helpful?
What can we do to improve the information ?