Technical FAQs

Ask a Question

What is reference of NSX Cord if System voltage is greater than 480Vac

The insulated NSX cord ref LV434204 is mandatory to be installed into the breaker instead the standard NSX chord if system voltage is greater than 480Vac.
Was this helpful?
What can we do to improve the information ?