Technical FAQs

Ask a Question

What is available wire range and number of wires for DC rated PowerPact LGL47100D40

This breaker parallels poles for ratings above 600A. Each pole accepts (2) 2/0 AWG–500 kcmil (70–240 mm2). So each leg of the circuit will accept four conductors, max 240 mm^2
Was this helpful?
What can we do to improve the information ?