Technical FAQs

Ask a Question

Can the Com'X 510 discover the devices that are locally connected to their Modbus serial port and downstream Modbus TCP/Modbus serial line gateways.

With the Modbus discovery function, the Com'X 510 can discover the devices that are
locally connected to their Modbus serial port and downstream Modbus TCP/Modbus serial
line gateways.
Was this helpful?
What can we do to improve the information ?