Technical FAQs

Ask a Question

How many device can be connected to EGX300 if working as Modbus TCP/IP Server

EGX300 allows maximum 64 connections concurrently from Modbus clients. 
This setting is also configurable from 16 to 64, the default Max is 32.
Was this helpful?
What can we do to improve the information ?