Technical FAQs

Ask a Question

Are Masterpact NT and NW suitable for 400HZ frequency

Masterpact NT and NW is not suitable for using at 400HZ Frequency because iron core CT which can be destroyed due to thermal
racing when it is working under 400Hz instead of 50/60 Hz.
Was this helpful?
What can we do to improve the information ?