Technical FAQs

Ask a Question

What is the peak inverse value of rectifier for N4 (380 Volt, three phase), M3 range (220V, three phase), and Y range (690V, three phase) in Altivar 71 drive.

The PIV value of rectifier is 1600V for N4 range. For M3 range, the PIV value is 800V and for Y range, the PIV value is 2200V. 
Was this helpful?
What can we do to improve the information ?