Technical FAQs

Ask a Question

Is the Relay common (R1C or R3C or R4C) are isolated from the Analogue Input common in ATV71 drive.

Yes, the Relay common (R1C or R3C or R4C) is isolated from the Analogue Input common.
The contacts of the relay are potential free and there is no physical contact of the relay common with the Analogue Input common.
Was this helpful?
What can we do to improve the information ?