Technical FAQs

Ask a Question

What devices will we be able to track and control via Smart Panel (e.g. Modbus, Ethernet, ULP).

Smart Panel will allow monitoring and controlling communicating devices that include the following:
• ACB and MCCB via IFE (Powerview Remote or an Electrical SCADA)
• MCB retail via Smart Link
• Local control via FDM128
Note: Comm'x 200 does not provide the ability to send controls
Smart Panel uses ULP as an event driven protocol. Modbus is used in a polling mode (i.e. does not support events, logging....).
Was this helpful?
What can we do to improve the information ?